Technical FAQs

Ask a Question

Customer has the 2510KR2 being used in a NEMA 3R mode, not NEMA 7&9. Can he get a replacement enclosure and is it the 9991KE3?

The customer can use the 9991KE3 but it is only NEMA 3R and not 3R/7/9. It will not be marked for use in a NEMA 7 & 9 hazardous location application.

CTA-ID : 2011131
Was this helpful?
What can we do to improve the information ?