Technical FAQs

Ask a Question

Can we provide bus connections from the main bus to the voltage transformers rather can cable connections?

Yes, we can provide bus connections from the main bus to the voltage transformers rather can cable connections. This would require drawout VTs and even then there will have to be a small piece of cable used. The terminals on the indoor type VTs are designed to accept cable connections only. The indoor VTs are used for most applications.

This application should be avoided if possible. It is not standard.


CTA-ID : 2011133
Was this helpful?
What can we do to improve the information ?