Technical FAQs

Ask a Question

Why would the product selector return two sections for an outdoor HVL/cc when only one switch was entered?

A single section for outdoor N3R HVL/cc is not available. The outdoor units need at least two sections for the roof and base channel. When adding on to a lineup, add two sections at a time.

CTA-ID : 2011130
Was this helpful?
What can we do to improve the information ?