Technical FAQs

Ask a Question

What should be done to meet this requirement a specification for silver plated bus joints?

All main bus is plated.
Aluminum bus is tin-plated as standard.
Copper bus is silver-plated and HVL and Visi/Vac.
Copper bus is tin-plated on HVL/cc.
Ground bus on HVL and Visi/Vac is silver-plated.
Ground bus on HVL/cc is bare.
Ground bus on HVL/cc with a plated requirement would be tin-plated.


CTA-ID : 2011377
Was this helpful?
What can we do to improve the information ?