Technical FAQs

Ask a Question

What is the operating time in cycles for Visi Vac circuit interrupters?<br />Contact Parting Time after energizing the trip coil.

The rated interrupting time of the Visi/Vac Circuit Interrupter is 3 cycles or 50 milliseconds.
The rated closing time is 5 cycles or 83 milliseconds.
The trip coil operates in approximately 1.8 cycles.
The close coil operates in approximately 3 cycles.
The motor operator recharges the springs in approximately 6 seconds.
Contact parting time after energizing trip coil is 1.2 cycles.

CTA-ID : 2011376
Was this helpful?
What can we do to improve the information ?