Technical FAQs

Ask a Question

Is there a parameter or some way to display the line voltage input into the unit using serial communication on the ATS48?


The unit does not have a feature which allows display of real time value of the line voltage via regular display nor serial communication.

CTA-ID : 2011370
Was this helpful?
What can we do to improve the information ?