Technical FAQs

Ask a Question

Do we offer RC snubber network and MOV protection on the input of the ATS46 unit?

We do have a RC snubber on the unit but do not offer MOV protection.

The ATS46 has a PIV of 1400 and due to design do not find it necessary to offer MOV protection.  

We do offer an application guide for overvoltage operation which discusses this and how MOV may provide a false sence of security.  The bulletin is 8638PD9602R12/97.


CTA-ID : 2011119
Was this helpful?
What can we do to improve the information ?