Technical FAQs

Ask a Question

Can the ATV58 unit be set up to operate using a second acceleration and deceleration above a certain hertz?


Go to menu 3. (drC drive menu)
Set parameter Frt (SwitchRamp2) to the frequency used to switch the second ramp.
Go to menu 2 (SEt Adjustments) to set up the ramp values.\
ACC & DEC are used between 0 and the Frt value.
AC2 and DE2 are used between the Frt and High speed.
The ramp rates are all based on 0 to Maximum frequency.

See keypad programming guide for additional information.

CTA-ID : 2011116
Was this helpful?
What can we do to improve the information ?