Technical FAQs

Ask a Question

Can you set the ATV66 unit up to automatically restart after a fault condition?

Yes.  You can go into menu 7.4 (fault management) and set up auto restart.

You can set unit up to reset by LI, Function key or manually reset.

The faults that can be set to automatically reset which desire are the following:
  AC Line overvoltage, DC bus overvoltage, Sequence time-out fault, Overspeed, Output phase loss, Drive overtemperature, Motor overload, Loss of follower, Process  time-out fault, serial link fault


CTA-ID : 2011115
Was this helpful?
What can we do to improve the information ?