Technical FAQs

Ask a Question

Is the 9002AW2 foot switch rated to ``turn-on`` and ``turn-off`` a motor directly?

Contacts are rated up to 10A continuously and NOT motor rated for direct starting of small motors.


CTA-ID : 2011359
Was this helpful?
What can we do to improve the information ?