Technical FAQs

Ask a Question

Can 2 sets of Roof Bushings be installed on a N3R outdoor HVL switch? One set for the line and one set for load.

Yes, 2 sets of roof bushings can be installed as long as nothing needs to be mounted in the rear of the enclosure.

One set is in the front over the line terminals of the switch and bus is run up to the top rear for the load bushings.

There are extra charges for the design of this feature.

CTA-ID : 2011355
Was this helpful?
What can we do to improve the information ?