Technical FAQs

Ask a Question

Is there a DC transient suppressor for 8501X relays, or can you use the 8501XS1 which the Digest says is for use on coils up to 120VAC?

That suppressor is rated for AC only, and it would not fit on the DC coil.


CTA-ID : 2011353
Was this helpful?
What can we do to improve the information ?