Technical FAQs

Ask a Question

What are the part numbers for the Speed Potentiometer assembly on the Class 8839 Econoflex drive unit?

31158-050-50 Potentiometer
ZB5AD922 Potentiometer operator
65170-166-44 Legend plate
ZBZ32 Legend plate holder


CTA-ID : 2011343
Was this helpful?
What can we do to improve the information ?