Technical FAQs

Ask a Question

What are the part numbers for the Hand-Off-Auto Selector Switch assembly on the Class 8839 Econoflex drive unit?

ZB5AD Three-position selector switch
ZB5AZ009 Mounting collar
ZBE203 Additional contact block (2 N.O.)
(2) ZBE102 Additional contact block (1 N.C.)
65170-166-17 Legend plate
ZBZ32 Legend Plate holder

CTA-ID : 2011342
Was this helpful?
What can we do to improve the information ?