Technical FAQs

Ask a Question

What are the part numbers for the AFC-Off-Bypass Switch assembly on the Class 8839 Econoflex drive unit?

ZB5AD3 Three-position selector switch
ZB5AZ103 Mounting collar with contact block (2 N.O.)
65170-166-43 Engraved legend plate ``AFC-Off-Bypass``
ZBZ32 Legend plate holder


CTA-ID : 2011339
Was this helpful?
What can we do to improve the information ?