Technical FAQs

Ask a Question

What is the difference between the 9001SKY1 and 9001SKY100 control station?

Issue:
What is the difference between the 9001SKY1 and 9001SKY100 control station?

Product Line:
Control Stations

Environment:
All products

Cause:
Product Features

Resolution:
9001SKY1 is single hole 30mm polymeric control station.  The 9001SKY100 is same control station with custom assembled operators.  Customer must furnish a 9001 Control Station Key Sheet with order.  Key sheet can be obtained from Customer Service or local field office. Also can be found in the Push button catalog 9001CT0001.


CTA-ID : 2010218
Was this helpful?
What can we do to improve the information ?