Technical FAQs

Ask a Question

What is the maximum number of jumper points available for a strip of 9080 Type G terminal blocks?

The comb style jumper strips used with the Type G blocks have a maximum of 6 poles. These jumper strips can be overlapped or daisy chained to extend the number of poles. Customer must be careful to not exceed the ratings of the terminal blocks or jumpers.


CTA-ID : 2008219
Was this helpful?
What can we do to improve the information ?