Technical FAQs

Ask a Question

Does the ATV28 unit have skip frequencies that can be set into the unit?

Issue:   Does the ATV28 unit have skip frequencies that can be set into the unit?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   This drive has one skip frequency that can be set in menu SEt.  The code for the parameter is JPF and operates at a range of 2hz around JPF setting.


 
Was this helpful?
What can we do to improve the information ?