Technical FAQs

Ask a Question

What is the heat sink fan part number for an ATV66U90N4U, ATV66D12N4U, ATV66U72M2U and ATV66U90M2U AC drive?

VZ3V663.

It is the heatsink fan located in the bottom of the drive. This part number is a kit consiting of both heatsink fans mounted together on a bracket.

The part # is listed on page 98 (page 104 in Adobe Acrobat) in the VD0C06S304E Receiving, Installation and Sart Up manual in Appendix A - Spare parts list. The part # for the cooling fans of the other size units is also listed in this table.


CTA-ID : 2006608
Was this helpful?
What can we do to improve the information ?