Technical FAQs

Ask a Question

Does the SU3040D400K come with two 200A 2P main breakers?

Yes. Unit comes with two Q2M2200VH main breakers factory installed. One 200A 2P feeds the 30/40 circuit load center in the unit. The other 200A 2P feeds an outside load.


CTA-ID : 2010158
Was this helpful?
What can we do to improve the information ?