Technical FAQs

Ask a Question

Can the ATV28 potentiometer start/stop option be removed because no longer want it and can the original cover be ordered?

Yes, it can be removed by unplugging and can then go to factory settings (FCS) in drive (drc) menu and run the unit normally.

The original face plate cover is not available to be ordered.

CTA-ID : 2009941
Was this helpful?
What can we do to improve the information ?