Technical FAQs

Ask a Question

Is the Econo-Flex ATV58 unit capable of having a second current limit setting that can have unit look at when want to switch using a dry contact?

The unit does not have a second current limit setting that can switch to using a dry contact.

The unit does have a second torque limit setting that can switch to using the a logic input when have the digital I/O option card installed.


CTA-ID : 2009700
Was this helpful?
What can we do to improve the information ?