Technical FAQs

Ask a Question

What is the mating cord for an L525WDR2M56?

The switch as shown has no connector. There is a 1/2`` NPT conduit entry.






CTA-ID : 2009694
Was this helpful?
What can we do to improve the information ?