Technical FAQs

Ask a Question

What is the temperature rating for 9037 float switch?

Temperature limitations for all float switches:
Ambient Minimum is -30 derees C (-22 degress F)
Maximum is 121 degrees C (250 degrees F)


CTA-ID : 2009693
Was this helpful?
What can we do to improve the information ?