Technical FAQs

Ask a Question

What is the replacement latch spring and pull ring for a QOC420LS load center cover?

Issue:
Repair Part

Product Line:
Obs QO LC Cover

Cause:
Maintenance

Resolution:
The latch spring is catalog number 40553-072-01.
The pull ring is part number 40553-073-01.
If a key operated cover lock attachment is required, use PK3FL. 


CTA-ID : 2009690
Was this helpful?
What can we do to improve the information ?