Technical FAQs

Ask a Question

Will 9001K62 work with 9001KR8, 9001KR8P, 9001KR9, 9001KR9P?

Issue:
Will 9001K62 work with 9001KR8, 9001KR8P, 9001KR9, 9001KR9P?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
Yes, it is for Type K and SK push-pull operators and illuminated push buttons and it holds the button in the depressed position and can be padlocked.


CTA-ID : 2010149
Was this helpful?
What can we do to improve the information ?