Technical FAQs

Ask a Question

What is the enclosure rating for the high HP Altivar 58 drives?

On the ATV58HC10N4X, ATV58HC13N4, ATV58HC15N4, ATV58HC19N4,U ATV58HC23N4, ATV58HC25N4, ATV58HC28N4, ATV58HC31N4 and ATV58HC33N4 the enclosure type is IP20 for all surfaces except the bottom. The bottom area is open. The power and control terminals at the bottom are exposed.


CTA-ID : 2009917
Was this helpful?
What can we do to improve the information ?