Technical FAQs

Ask a Question

What are the part number for the QOU breaker wire binding screws

Below 30A they are not available.
Part number 48820-015-01 for ``high amp:``
QOU180 QOU190 QOU1100 QOU280 QOU290 QOU2100 QOU2125
QOU370 QOU380 QOU390 QOU3100

Number: 48820-078-03, for low amp
QOU110 QOU115 QOU115HM QOU120 QOU120HM QOU125 QOU130 QOU135 QOU140 QOU145 QOU150 QOU160 QOU170 QOU210 QOU215 QOU220 QOU225 QOU230 QOU235 QOU240 QOU245 QOU250 QOU260 QOU270 QOU215H QOU220H OU225H QOU230H QOU310 QOU315 QOU320 QOU325 QOU330 QOU335 QOU340 QOU345 QOU350 QOU360


CTA-ID : 2009679
Was this helpful?
What can we do to improve the information ?