Technical FAQs

Ask a Question

Is there a defeat mechanism on the 9421 Type N operator for opening the door with it in the ON position?

Yes there is. This is a requirement of UL98 and since this switch meets UL98 requirements, it has a defeat mechanism.

CTA-ID : 2009671
Was this helpful?
What can we do to improve the information ?