Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H326NAWK Heavy Duty safety switch?

The lugs on this device will accept TWO #3 AWG - 500 kcmil aluminum or copper conductors per phase and neutral.


CTA-ID : 2010143
Was this helpful?
What can we do to improve the information ?