Technical FAQs

Ask a Question

Can an NQOD430M100CU be converted to a main lug only panel?

Could use a QOB3125SL in place of the back fed QOB3100. The NQOD430M100CU has studs to accept main lugs but the lugs are not available in a standard conversion kit available from stock.


CTA-ID : 2010139
Was this helpful?
What can we do to improve the information ?