Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATS48D62Y, ATS48D75Y, ATS48D88Y, or ATS48C11Y soft starter?

The entire width of the unit is a = 7.48 in (190 mm), the entire height of unit is b = 11.42 in (290 mm), the entire depth of the unit is c = 9.25 in (235 mm), and the weight is 18.3 lb (8.3 kg).

See the associated literature for additional details regarding mounting of this soft starter unit.


CTA-ID : 2010133
Was this helpful?
What can we do to improve the information ?