Technical FAQs

Ask a Question

What is the part number for the Dynamic Braking Resistor for the ATV28HD23N4U?

The part number is VW3A66713.

The list of enitire line of db kits for the ATV28 is in unit`s catalog 8840CT which is accessible on the Square D internet in the Technical Libray under Panel Drives and ATV28 Catalogs and Pricing.


CTA-ID : 2009900
Was this helpful?
What can we do to improve the information ?