Technical FAQs

Ask a Question

What is the part number for Lonworks module for the Altivar 58?

The part number is VW3A58312PU.
The keypad port can be used to connect to the Lonworks module or it can connect to a VW3A58303U Modbus card.
Also, a 24V DC power supply (140mA) is needed to provide power for the Lonworks module.
It is not recommended to use the +24 and COM on the drive to provide this power.


CTA-ID : 2010362
Was this helpful?
What can we do to improve the information ?