Technical FAQs

Ask a Question

Will a 12 VDC signal work on LI1?

This is not recommended.
The signal must be 15Vdc +/- 15% to operate the Logic inputs.
Positive logic: state = 0 if < 5 V, state = 1 if > 11 V.
Using a 12 VDC power supply for logic inputs may not povide relable input signals to the drive.


CTA-ID : 2010357
Was this helpful?
What can we do to improve the information ?