Technical FAQs

Ask a Question

What is the enclosure cooling fan part number for the 50 hp 460v 8839 66UPG4CC?

This is the seven inch enclosure fan and the part number is 26016-31100.

This same 7`` fan is used for the following enclosures and has a quantity of two (Qty 2) per enclosure:
25-40 HP CT
25-40 HP VTLN
30-50 HP VT
50-75 HP CT
50-75 HP VTLN
60-100 HP VT
100-200 HP CT
125-200 HP VT


CTA-ID : 2010126
Was this helpful?
What can we do to improve the information ?