Technical FAQs

Ask a Question

Can 2- wire inductive sensors be wired in parallel?

The use of 2 wire proximity sensors wired in parallel either across themselves or together with dry contacts is not recommend. When the 1st sensor turns on it will short out the other sensors.

CTA-ID : 2010013
Was this helpful?
What can we do to improve the information ?