Technical FAQs

Ask a Question

Is the 9423M660 lock bar kit meant to be cut?

The lock bar kit contains two ``Universal Lock Bars`` which covers all the door openings between 40`` and 60``. The bars are finished on one end and blank on the other.
Simply measure the enclosure door opening and cut per the following formula and modify as shown:

A/2 + .313 = L

A = Measured enclosure door opening
L = Length of lock bar

CTA-ID : 2010120
Was this helpful?
What can we do to improve the information ?