Technical FAQs

Ask a Question

Is the 9001KPZ1 Nema type 1 Control station with pull box Flush mounted ?

Yes it is, See page 16-104 Digest 172


CTA-ID : 2009895
Was this helpful?
What can we do to improve the information ?