Technical FAQs

Ask a Question

What is the part number for directory cards for QMB panelboards?

The standard directory card that fits into the plastic pocket and is numbered 1-54 is part number 80031-158-01. The part number for directory card numbered 43-96 is 80031-158-02. The plastic pouch part number is 80031-159-01.

CTA-ID : 2009887
Was this helpful?
What can we do to improve the information ?