Technical FAQs

Ask a Question

What is the maximum branch breaker and/or maximum back fed main breaker that can be installed in the QO612L100RB or QO816L100RB Load Center?

Issue:
Application

Product Line:
QO Load Center

Cause:
Confirmation

Resolution:
The wiring diagram will state to use 70A maximum branch breaker or 100A maximum back fed main breaker. When a back fed main breaker in installed, the PK2MB retaining kit must also be used. 
This is also applicable for the QO612L100TRB and QO816L100TRB Load Centers. 


CTA-ID : 2009885
Was this helpful?
What can we do to improve the information ?