Technical FAQs

Ask a Question

What is pay back period of the incremental cost adder of a Type EE energy efficient transformer over a standard general purpose transformer (new installation)?

NEMA estimated the payback period of transformers that meet NEMA Standard TP 1-1996 (SqD Type EE) over general purpose transformers to be approximately 3 years when applied with a 35% duty cycle and a kwh rate of $0.065.  For more detailed discussion, contact Product Marketing.


CTA-ID : 2009881
Was this helpful?
What can we do to improve the information ?