Technical FAQs

Ask a Question

Can`t get 8839 58E Econoflex with Metasys to run at greater that LSP? Using serial communications to command the drive.

Discovered that the bulletin No. 300072-450-10G does not make it clear what to do with LI4 and thus may have it programmed for forced Local with the factory installed jumper on it and using serial communication.

Remove jumper and unit works fine because no longer being told to look at terminal in forced local condition.

CTA-ID : 2010354
Was this helpful?
What can we do to improve the information ?