Technical FAQs

Ask a Question

Can you get 42K AIC or 100K AIC using a KC circuit breaker with the ATS48?

No.

You can not get above 30,000 AIC rating with the use of the circuit breaker.

To get above the 30,000 AIC rating you must use recommended fuses to get this co-ordination.


CTA-ID : 2010344
Was this helpful?
What can we do to improve the information ?