Technical FAQs

Ask a Question

Does the ATS46C11Y have connections for the KM3 user supplied shorting contactor?

Yes it does have connections A1, B1, C1 and A2, B2, C2 per Manual VD0C32S301B (June 1998) page 17. The R2 relay contacts can be used to close the shorting contactor at end of start and open the contactor for stopping the motor. The wiring diagram on page 22 shows the wiring diagram.


CTA-ID : 2010342
Was this helpful?
What can we do to improve the information ?