Technical FAQs

Ask a Question

What are the physical dimensions of a QMB3400LA?

The only meaningful dimension is the 7.5`` of mounting height. The version of panelboard/switchhboard will determine if this switch can be used. REFER TO THE SUPPLEMENTAL DIGEST.


CTA-ID : 2010340
Was this helpful?
What can we do to improve the information ?