Technical FAQs

Ask a Question

Does Square D offer transformer vibration isolation pads?

Square D does not offer external transformer vibration isolation pads. Square D`s low voltage dry type distribution transformers have vibration isolation pads between the core and coil assembly and the enclosure. Square D recommends that the enclosure be solidly bolted to the largest mass possible to minimize audible noise. Should the customer choose to not follow this recommendation, then vibration isolation pads can be obtained from Korfund, Mason, or Goodyear (there are other suppliers in the industry as well).

CTA-ID : 1814
Was this helpful?
What can we do to improve the information ?