Technical FAQs

Ask a Question

Is there a logic output contact on the ATV11 unit that can be used to indicate drive running?

Yes.  The DO output can be used as a logic output that can be assigned to frequency threshold attained - FtA.
When the motor frequency exceeds frequency assigned in the Ftd parameter the logic output is closed ( state of 1 ).  Thus can set Ftd to 1 hz and then when motor fequency exceeds this the output is closed.

CTA-ID : 2009878
Was this helpful?
What can we do to improve the information ?