Technical FAQs

Ask a Question

Can the option C08 ( light cluster Red power on, Green AFC run & Yellow AFC Fault ) be used with the A07 ( Hand / Off / Auto , Speed Potentiometer) on the 883958E?

No the C08 option can not be used A07 ( HOA, Speed Pot ), or B07 ( Hand / off / Auto , Start / Stop , Speed Potentiometer).


CTA-ID : 2009873
Was this helpful?
What can we do to improve the information ?