Technical FAQs

Ask a Question

Do Zelio Logic relays generate any signal or switching frequency above 100 mega Hz? Concerned with interference with computers or other sensitive electronics

Maximum operating rate .5 hz at load
10 hz without load
Maximum counting frequency 60 hz



CTA-ID : 2009872
Was this helpful?
What can we do to improve the information ?